Locate a Dealer » Become a Dealer » Dealers Portal » Developers »
Toshiba Telecommunication Systems Division


Brookhaven Memorial Saves More Than $400,000 The First Year With Toshiba VoIP System

MISSION: Cut Phone Costs; Improve User Experience; Maintain 24/7 Reliability
Don Fleming, CIO, and Scott Weber, telecom manager, at Brookhaven Memorial, specified a system that would:

Brookhaven’s IT team turned to Black Box Network Services of Amityville, New York, an Authorized Toshiba Dealer for more than 30 years.

Chris Gibbons, VP of Black Box Network Services of Amityville, New York, recommended Toshiba’s Strata® CIX™ business communication system.

Toshiba backs up its reliability with the industry’s longest manufacturer’s extended warranty, allowing customers to build the warranty into the overall cost of the system.

Fleming and Weber were already sold on Toshiba as the hospital had used Toshiba telecom systems since the early 1990s. In fact, Black Box has been the hospital’s Authorized Toshiba Dealer for more than 20 years.

Solution: Toshiba Strata CIX Exceeds Hospital’s Goals
Installed by Black Box Network Services, Brookhaven Memorial has a network of Strata CIX IP business telephone systems at seven locations throughout the East Patchogue, New York area. The system includes:

All the systems are networked together over IP using Toshiba’s Strata Net.

Result #1: Remote Administration for More Control
Using Toshiba’s Network eManager® remote administration tool, Weber can now remotely manage the entire telephone system from his desk. He can also troubleshoot issues more effectively since he has more control over the system.

Weber said, “I am no longer at the mercy of the telephone company to fix problems or make changes. I can now administrate the system from my desktop and make moves, adds and changes on the fly without waiting for a service call and without any service charges.”

Result #2: Improved User Experience
Now with the new Strata CIX system, hospital personnel can easily program telephone features and integrate with other applications such as Microsoft® OCS. They can facilitate Unified Messaging and receive their faxes on their computers along with their emails and voice messages. The system has also enabled direct extension dialing, caller ID and message waiting lights, all of which help improve efficiently.

“With the new system, everything is easier and more intuitive for our employees, which helps them be more efficient and lessens the load on the IT team to keep things working,” Weber said.

Result #3: Unified Messaging Improves User Experience
Brookhaven Memorial eliminated $22,000 in monthly Centrex costs by moving to PRI lines and reducing costs for maintenance. It also reduced the pressure on the network capacity.

In addition, migrating from older Toshiba Strata DK484 systems saved the hospital in excess of $150,000 over buying a new system. Staying with Toshiba allowed it to re-use its existing digital and analog telephones as well as system cards.

Bottom Line: $110,000 Savings the First Year; $10,000 Savings Annually Thereafter
Toshiba’s Strata CIX IP business telephone system has helped Brookhaven Memorial meet its goal of reducing its communication costs, improving user experience, and providing exceptional reliability.

Brookhaven Memorial savings includes:

For an Authorized Toshiba Dealer, Visit: www.telecom.toshiba.com