2008 Press Releases
Toshiba Strata CIX1200 VoIP Business Communication System Brings Toshiba Quality, Reliability and Affordability to 1,152-Port Market

IRVINE, Calif., August 12, 2008 —Toshiba America Information Systems Inc., Telecommunication Systems Division (Toshiba — www.telecom.toshiba.com) today announced the launch of its new Strata® CIX™1200 VoIP business communication system, bringing Toshiba quality, reliability and affordability to medium-to-large companies. Supporting up to 1,152 ports, the Strata CIX1200 is designed for 200 to 1,000 users and delivers networked applications for as many as 128 sites.

“The new Strata CIX1200 expands Toshiba’s reach in the medium-to-large market segment, giving enterprises a robust Toshiba solution at nearly double the port capacity of our Strata CIX670,” said Brian Metherell, vice president and general manager. “As with the entire Strata CIX family, the new Strata CIX1200 gives users Toshiba’s legendary quality and reliability in an affordable VoIP system that can be networked with up to 128 sites. The CIX1200 can be customized using Toshiba’s FeatureFlex® adapatability tool, and provides a smooth migration path from smaller Toshiba systems.”

Strata CIX1200 Is the Only 1,000+-Port System to Offer User Customization
Toshiba’s Strata CIX1200 is the only system of its size to allow the user to adapt capabilities to their specific needs. Using FeatureFlex, Toshiba’s feature adaptability and customization tool, the system can be tailored well beyond its standard system features, administrative options and programmable features. It allows enterprises to create user-definable features companywide, by department, or for individual users. Existing features can be modified, and new ones can be created, including features in CIX call processing, as well as blended features that work between all system applications and resources.

“FeatureFlex allows users to customize their own individual features to help them be more efficient with their communications solution,” said Shahin Hatamian, vice president of Product Management. “FeatureFlex makes the resources of the system available to create new or blended features and applications.” The CIX1200 contains the same feature-rich functionality as existing Strata CIX communication systems.

Strata CIX1200 Can Be Networked up to 128 Sites
Strata CIX1200 can be networked with other Toshiba Strata CIX systems, from other CIX1200s all the way down to the small 40-port Strata CIX40. It can be networked for up to a total of 128 sites to accommodate larger capacity or distributed configurations.

“The Strata CIX1200’s networking capabilities make it a perfect solution for a headquarters site that is networked to small or remote offices or retail/restaurant locations,” said Bob Lerche, product manager.

Easy Migration to Strata CIX1200 From Other Toshiba Strata CIX Systems
Toshiba has retained its renowned migration path with the Strata CIX1200. Users of other Toshiba Strata business communication systems can easily migrate their systems to the new Strata CIX1200. Telephones and almost all system interface cards may be re-used as well as voice mail systems and the Strata MAS with resident applications. Providing a smooth migration path gives users the ability to retain much of their original investments, while they gain the benefits of the larger system and its additional capabilities.

All Applications on a Single Server Delivers Clean Integration, Affordability
Toshiba Strata CIX1200 and all other Strata CIX models are compatible with Toshiba’s Strata Media Application Server (Strata MAS), which delivers valueadded application processing. Strata MAS is one of the first application servers to use Host Media Processor (HMP) technology resources as an alternative to Dialogic boards in the server. HMP is more cost-effective and does not require card slots, making the server more compact and potentially trouble free.

Strata MAS integrates all value added applications such as voice mail/unified messaging, IVR, ACD and reporting, Video Conferencing and Collaboration, Web-based Personal and System Administration, and FeatureFlex™ customization tools all on one platform. This provides better application integration and significant cost savings over designs that require separate servers for each application.

New Large-Capacity Voice Processing System Also Introduced
For voice mail/unified messaging applications requiring more than 32 ports, a new IP-based voice processing system called Stratagy ES96i will soon be available to provide 96-port capacity in an industrial-grade rack-mount server with an Intel Xeon processor and dual redundant power supplies standard. RAID1 or RAID5 hard drive redundancy options are available in addition to the other value-added applications, which include Fax Integration, Interactive Voice Response, Automatic Speech Recognition, Text-to-speech, FeatureFlex™ adaptability tools, Network eManager™ system administration and My Phone Manager™ personal administration.

Features in the Strata CIX1200 include:
  1. Strata Net Networking — Strata CIX1200 can be networked with all of Toshiba’s Strata CIX family, including the CIX40, CIX100, CIX200, CIX670, and other CIX1200 systems. This allows large companies to use the Strata CIX1200 for their main sites, and smaller Strata CIX systems for branch offices or other remote locations, as well as allows smaller companies to expand as they grow
  2. Virtually All Features to All Toshiba Users, on Fixed or Mobile Devices — Strata CIX1200 and the other Strata CIX models have been designed to deliver virtually every feature to every user, regardless of the type of Toshiba endpoint being used, whether they are fixed or mobile. The system supports IP telephones, IP wireless telephones, IP soft phones on notebook and tablet PCs, and digital (TDM) and analog telephones
  3. Choice of Endpoints — Strata CIX1200 and all Strata CIX systems are compatible with Toshiba’s IP and digital telephones, including Toshiba’s new IP5000 IP telephones, Attendant Consoles, Toshiba SoftIPT® soft phone for laptops and PDAs, and third-party SIP telephones (as tested by Toshiba)
  4. Traditional Business Telephone Features in an IP System — Strata CIX1200 delivers virtually all the features and functionality of Toshiba’s traditional digital business telephone systems, taking advantage of decades of experience serving enterprises with voice solutions
  5. Ability to Mix and Match IP and Digital on a Single System — Unlike many competitive IP systems, Strata CIX1200 can be TDM-enabled, giving users a choice of running a pure IP system or a mix of IP and digital TDM. This allows users to choose how they will maximize their systems and migrate existing equipment
  6. Strata Media Application Server (MAS) Compatibility — Multiple applications can be combined on a single media application server platform. Applications include Auto Attendant, Voice Mail, Unified Messaging, Fax Integration, Automated Speech Recognition, Text to Speech, Interactive Voice Response, Automatic Call Distribution and Reporting, Web-based Personal and System Administration, Web-based Telephone Applications, FeatureFlex™ adaptability tool that allows users to customize and add features, and other third party applications. Strata MAS comes standard with Toshiba’s Voice Processing/unified messaging solution, My Phone Manager™ personal administration tool, and eManager™ system administration tool
  7. Video Communication Solution (VCS®) Compatibility – Toshiba’s VCS provides affordable point-to-point video conferencing, desktop/application sharing, file transfer and message board capabilities for up to three parties.

To find an Authorized Toshiba Dealer in your area, visit the Toshiba website at:
www.telecom.toshiba.com.

About Toshiba America Information Systems Inc. (TAIS)
Headquartered in Irvine, Calif., TAIS is comprised of four business units: Digital Products Division, Imaging Systems Division, Storage Device Division, and Telecommunication Systems Division. Together, these divisions provide mobile products and solutions, including industry leading portable computers; projectors; imaging products for the security, medical and manufacturing markets; storage products for automotive, computer and consumer electronics applications; and telephony equipment and associated applications.

TAIS provides sales, marketing and services for its wide range of information products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, which is a global leader in high technology and integrated manufacturing of electrical and electronic components, products and systems, as well as major infrastructure systems. Toshiba was founded in 1875, and today operates a global network of more than 740 companies, with 198,000 employees worldwide and annual sales surpassing US$76 billion. For more information on Toshiba’s leading innovations, visit the company’s Web site at www.toshiba.com.

###

© 2008 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice.


©2009 Toshiba America Information Systems. All rights reserved.    
Toshiba Worldwide | Toshiba America | Terms of Use | Privacy Policy | Site Map