Application Portal

Toshiba and its partners provide various applications to address customer's specific needs. Here is the list of applications created for Toshiba systems.

Market Segment: General
Application Description System Technology Vendor
FF Call Monitor After not answering your telephone, you can listen to a caller now leaving a voice message. During this message recording process, you can connect to the caller immediately to talk in real time or let the caller finish leaving the message. Call Monitor provides the flexibility of handling the call now or later. Strata CIX/MAS FeatureFlex Toshiba
FF Call Return While listening to your voice message, you can return the call immediately. When the call is finished, you immediately return to the position in the voice mail listening queue where you were and continue listening to the voice messages. Strata CIX/MAS FeatureFlex Toshiba
FF One Number Access Incoming calls to your number route to your desk telephone, then cell phone, etc. until it finds you. If you don’t answer, at any of the programmed destinations, your office voice mail takes the message. The intelligent routing to any destination and only having one voice mail to check is what provides the efficiency and value. Strata CIX/MAS FeatureFlex Toshiba
FF Call Screen You can answer important calls only while letting other calls go to voice mail to leave a message. Announcing the caller name and Caller ID enables you to make the choice depending upon the caller. You can create an accept list and a reject list easily from your web browser using My Phone Manager. Call Screening is activated from your telephone, so when you are busy, just press the button on your desk phone, then you receive calls only from your important callers. Strata CIX/MAS FeatureFlex Toshiba
FF Alarm Clock A reminder feature for your digital telephone is user programmable, so at the prescribed time, the system calls your telephone and plays the announcement call and displays the message on the LCD. Strata CIX/MAS FeatureFlex Toshiba
FF Hot Desk Multiple users can share digital telephones to provide a cost effective operation for a shared office environment. Users can sign into any telephone it will assume their programmed directory number, feature operation, and personal telephone preferences. Hot Desk functionality is also supported on IP telephones, but through the Strata CIX software rather than this FeatureFlex application. Strata CIX/MAS FeatureFlex Toshiba
FF Simultaneous Ringing Calls ring both on your desk telephone and mobile device (cell phone, wireless LAN mobile phone, home phone, or another extension in the system), enabling you to answer from either phone, depending on whether you are at or away from your desk. This provides desk telephone convenience and cell phone mobility. Strata CIX/MAS FeatureFlex Toshiba
FF Personal Call Handling User definable parameters combine the features of schedule-based call and caller-based routing of incoming calls, one number access (find me follow me sequential ringing), call screening (announcing the caller name), and simultaneous ringing of desk and mobile phones. This insures the most expeditious handling of your incoming calls. Strata CIX/MAS FeatureFlex Toshiba
FF Security Code Update The system prompts the user to change their mailbox security code at a specified interval to provide better voice mail security. The interval can be a specified number of days, weeks, months or years. By forcing the user to frequently change their password, the voice mail system will be less vulnerable to intrusion due to compromised passwords. Strata CIX/MAS FeatureFlex Toshiba
InfoManager News The application allows the end user to create a message tha dt can be sent to every phone in the company. The message will appear on the screen until the end user turns it off. It’s a quick and easy way to communicate simple messages to employees. IPT2008 InfoManager Toshiba
InfoManager Calendar The application llows the end user to track their meetings for the day using the Outlook Calendar View. IPT2008 InfoManager Toshiba
InfoManager Stock Quote The application allows the end user to assign a button that will show stock quotes when pressed—a simple and easy way to stay informed using the large screen telephone IPT2008 InfoManager Toshiba
InfoManager Weather The application allows the end user to download current weather information from the Internet. IPT2008 InfoManager Toshiba


©2010 Toshiba America Information Systems. All rights reserved.    
Toshiba Worldwide | Toshiba America | Terms of Use | Privacy Policy | Site Map